HI
1.Could you help check the BQ24133 schematic as below and any need to adjust
2.Q1 can be changed to DIODE? ACDRV and CMSRC be Floating?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
1.Could you help check the BQ24133 schematic as below and any need to adjust
2.Q1 can be changed to DIODE? ACDRV and CMSRC be Floating?
Gareth,
Please review the documents below. Let me know if you have any further questions.
Best Regards,
Ricardo
Hi Ricardo
would like to ask BQ24133 STAT status. At present, the circuit will use STAT to connect to LED to display the two statuses of battery charging and charging completion. Use BQ24133 EVM to verify that a and b function normally, but the battery is fully charged and STAT is still Low. CE is used to control the EVM. , If there is no MCU to control CE, how do I make STAT be H after charging?
Gareth,
You have disabled charge termination by pulling TTC to LOW. When termination is disabled, the charger will not terminate autonomously and external circuitry or a host control will need to disabled charging by pulling ISET to LOW.
Best Regards,
Ricardo