Other Parts Discussed in Thread: , TPS62825
Hi Team,
The output voltage of LM27761EVM is set to -2,7V by changing R1 to 200k and R2 to 160k, when the input voltage is 3V and output current is 200mA, the output voltage will increase to -2.4V which cannot be accepted by the load.
May I ask if there is any work-round solution to have LM27761 output voltage to be stable at -2.7V when the output current is 200mA and input voltage is 3V? The input voltage cannot be increased for this application.
If not, could you please help recommend alternate device?
Thanks and Best Regards!
Hao