This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23610-Q1: Voltage Drop

Part Number: LMR23610-Q1

Hi,

I am using LMR23610-Q1 as follows:

Vin= 5.5 to 27 V

Fsw= 2 kHz sync with external clock

Iout = 0.4A

Vout = 5.5V

I am worried about what would happen at Vin_min = 5.5V. What would be the Vdrop across the IC and what Vout whould I get?

What would be the minimum Vin to get Vout= 5.5V in the given conditions?

Thank you