Other Parts Discussed in Thread: LM5157, TPS55340,
Tool/software: WEBENCH® Design Tools
Dear support Team,
I am looking for a DC/DC step-up converter and Webench proposed to me the LM5157 & LM51571 chips.
Design: supply input 20 V to 25V / supply out 34V / current max 3A / 40°C temperature integrated transistor
I made the simulation with Webench and I get a capacitor for Cout "custom" Cap= 3.01868 uF / ESR= 1.0 uOhm / VDC= 51.0 V / IRMS= 3.7022 A
This is quite strange as usually Webench use "real" devices for it's simulation, so it why I am contacting you.
After this simulation I check the datasheet of the chip and I saw that this one is realy new and only preview stage.
Can you tell me when this chip will be release as I am planing a small redesign of an existing board?
Concerning the Webench simulation, can you told me if there wrong in Webench concerning this chip?
Many thanks for your help.
Best Regards,
Xavier