Hi team,
We have some questions about testing method for LP5910 LDO PSRR,
- The complete circuit
- The input signal source (instrument, amplitude of ripple setup)
- Measurement of the output
Do we have related APP note mention this setup?
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We have some questions about testing method for LP5910 LDO PSRR,
Do we have related APP note mention this setup?
Regards,
Roy
Hi Roy,
Here are some app notes which discuss measuring PSRR in general.
https://www.ti.com/lit/an/slaa414a/slaa414a.pdf
https://www.ti.com/lit/an/slyt547/slyt547.pdf
https://www.omicron-lab.com/fileadmin/assets/Bode_100/ApplicationNotes/PSRR/App_Note_PSRR_2_0.pdf
When I measure PSRR I use the Omicron Bode 100 with the Line Injector module from Picotest. This assumes that the LDO does not require an input capacitor. If the LDO requires an input capacitor then you need a different method such as what is used in the first app note I provided, as the Bode 100 + line injector are not capable of driving the capacitor at high frequencies while maintaining the injection level.
Thanks,
- Stephen
Also, attached is a quick ppt with a block diagram of the setup and things to watch out for.
Hi Kyle,
We would like to use TINA to get the PSRR response. But the result doesn't match to datasheet. Our TINA file is as below, could you let me know the setup and simulation step?
Roy
Hi Roy,
The simulation looks correct to me. Here are the results. The TI legacy simulation models are accurate with regards to the typical DC attenuation, the first pole and the first zero. You can see that they used about -80 dB as the DC attenuation, followed by a pole at around 1 kHz and a zero around 200 kHz. This approximates what you see in the datasheet in figures 11, 12 and 13.
Thanks,
- Stephen