Other Parts Discussed in Thread: LM5069
I have an evaluation board LM5069EVM-627 surge stopper and reverse voltage protection. To turn it on and off, I would like to use a signal from an MCU (3.3V) that would switch, a MOSFET (2N7002), just like on the LM5069 datasheet figure 26. I would connect the source from the MOSFET to the same GND as the LM5069.
Could there be any problems due to the connection of GND to SGND via diode D1. My design is 24V / 22 A Hot Swap.
Regards,
Davorin Kotnik