This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40425: BP5 for power stage

Part Number: TPS40425

Hello TI,

In my design I am using TPS40425 and the power stage is CSD95372A.

The design spec is: 

12V input, 0.85V output @50A dual phase operation.

The power stage CSD95372A needs 5V for VDD (gate drive), I would like to know whether can I use TPS40425 internal 5V LDO (BP5) to supply 5V to CSD95372A?

Thanks in advance.

Regards,

Srinivas