Hello,
I a design, a TLV62130 is used to create a 3.2V voltage supply.
Probing the SW pins I see the waveform below during operation.
I am wondering why there is this sine waveform before the square pulse.
Any idea ?
Best regards,
Stéphane
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I a design, a TLV62130 is used to create a 3.2V voltage supply.
Probing the SW pins I see the waveform below during operation.
I am wondering why there is this sine waveform before the square pulse.
Any idea ?
Best regards,
Stéphane
Stephan,
It appears to me that your design is running in "Power Save Mode" (Discontinuous mode) and the sine wave you are seeing on the SW pin above is the expected behavior as the internal low side FET is disabled when the inductor current drops to zero.
You can see this same behavior illustrated in figure 35 in the datasheet, although the duty cycle is less than in your design.
Sincerely,
-Matt
Hello Mat,
Thank you for your answer Matt.
I will add a load to try moving out of power save mode.
Regards,
Stéphane
Stephane,
Please be aware that there are traditionally no problems with having the DC/C regulator run in discontinuous mode. The device is specifically design to run in this mode to maximize the efficiency at light loads. Although, there are some applications that may have a problem with the change in frequency that corresponds with the Power Save mode.
Thus, if you do need to keep the device out of discontinuous operation, you may also try increasing the inductor value since the transition to Power Save mode occurs when the output load current drop below 1/2 the inductor ripple current.
Sincerely,
-Matt