rt Number: UC2842
Hi, Ti member
We are developing the buck converter based on UC2842. Instead of current mode, use voltage mode refer datasheet and add additional OPA circuit to limit output current.
there are a compensated circuit cascade a diode to limit Vcomp by internal current source of IC and Isense-Pin injected a Ramp signal by RT,CT. (Vcomp compared to Isense to produce a PWM signal)
the parameter setup:
1. OSC frequency is 8%
2. Isensn Ramp range: 90mV --> 920mV
but the minimum duty is 8% , it very hard to control output current at short condition.
Ch1: output current , Ch3: Vds ,Ch4: Vgs
we tune a lot of ways to limit duty :
1. change Isense Range
2. Vcomp value by DC source
3. OSC frequency
above all ,the minimum duty still keep 8% . Could you tell me how to do can limit PWM below 1%?