Hello
I would have a question about BQ25504 ultra low-power boost converter. In the data sheet of the device, the minimum starting voltage is 600mV but no information about the minimum input current. In the circuit I will design, the input current is at the microampere level. My input voltage value is maximum 600mv. What will be my output voltage and current in these input values? Also, can the battery be charged with these values?
Is there any source I can test this device in the simulation environment?
Thanks in advance for your help.