This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS56428: Simulation does not start

Part Number: TPS56428

Tool/software: WEBENCH® Design Tools

Hi,

I simulate TPS56428 on VIN=5V, VOUT=3.3V, IOUT=4A condition, however it is not executed as below.

 

Why is it?

Best Regards,

Kuramochi

  • Hi,

    I think WEBENCH set a duty limit here,~65%. But it should be okay with higher duty , as the max duty is around 83% , based on the(1- minoff time / cycle time ).

    if you need a WEBENCH quick results, you can "input" 5.2Vin to check.

    BRs,

    Young