Other Parts Discussed in Thread: ADS1235, , ADS1261, LMR33630
Hello
I'm working on a project for a load cell data acquisition using the ADS1235 for data reading. In this scenario i have only the input voltage of 24VDC, then i need to generate a 5V and a 3.3V for powering the circuit and the load cell (AVCC / DVCC). I'm searching for the best solution for a high quality power supply, with the lowest levels of noises and EMI. I found the TPSM53602 witch is a general propose power supply with several advantages, but i couldn't find any application or examples on ADC circuits. I'd like to know if it's a good solution. My plan is to use two of these. One for 5 and 3.3 V.