Hi there,
Is it possible to use 2.2uF cap. with 10Vdc rating on between CFLY1 and CFLY2 pin? This cap. is a charge pump cap. for negative output. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
Is it possible to use 2.2uF cap. with 10Vdc rating on between CFLY1 and CFLY2 pin? This cap. is a charge pump cap. for negative output. Thanks.
Hello Alan,
As shown in the datasheet typical application circuits, using a 2.2uF capacitor is ok for low current (<40mA) applications but a 4.7uF capacitor is recommended for higher current applications (>40mA). Also, a 16V or higher rated capacitor is recommended because of possible overlap of switching states as well higher DC biased capacitor value.
Kind Regards,
Liaqat