Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84212: When Vin is lower than 14.5V, what is the output?

Part Number: TPSM84212

Hi Team,

The minimum of input is 14.5V in TPSM84212EAB..If the input is 12V or less than 12V, will the output follow input.

 customer could accept such situation A. For example, Vin =12V, Vout =11.9V.

But if Vin =12V, Vout =0V, customer can't accept.