This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754: tps23754 design problem

Part Number: TPS23754
Other Parts Discussed in Thread: TPS23756, TPS23730

     I used tps23754 to design a POE function board, isolated output DC12V.

     Because I also need a DC24V adapter in,  according to document slva306a ,I select option2   .however ,in this case ,only DC33V+ can works normal ,out12V .  IF adapter=24V ,the output is only 8V..

    So how to change my design to meet out request?

    thanks  I need your help.SCHEMATIC1 _ 1.pdf

     

  • Hello,

    You need to use the TPS23756 or TPS23730 that has PPD which enables lower turn on voltages. Please review their reference designs and EVM's.

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments