This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429: Confirmation of feasibility

Part Number: LM3429
Other Parts Discussed in Thread: TPS92691, TPS92692

Hi support team,

Is it feasible with the boost of LM3429 with the following specifications?

 

- Vin: 8 ~ 36.5V

- LED IF: 55mA

- LED VF: 2.85V

- Number of LEDs: 18

- Dimming signal: Duty 0~100%, 11±3V, 190Hz±20%

 

LED: NICHIA, NFSW757GT-V3

https://www.nichia.co.jp/specification/products/led_spec/NFSW757GT-V3-E(5466)Rs030.pdf

 

Regards,

Dice-K