This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM72445: 'SM72445' Inquiries about abnormal operation at low power.

Part Number: SM72445


Hi, TI expert.

A customer company is developing it using 'SM72445', but in case of low power, an abnormal operation occurred and inquired.

The circuit is said to be configured the same as the EVM Board in the attached file.

The contents of the inquiry are as follows.

* When input 45V is applied, the following waveform is measured.

* 1V is measured on the VIIN pin of SM72445, causing abnormal operation at low power.

It is said that the same phenomenon occurs on the EVM Board. (See waveform below)

We request a software solution review for this issue.

- AIIN pin voltage floating phenomenon related

   - Each Analog Value Offset can be set in Reg4 by using I2C.

   - I looked up the contents of the field, but there is no other content other than the above.

(Questions)

1. Is it 8bit hex data, can I understand 1bit as 5V / 1024 Sampling?

2. Is 8bit Data Unsigned? Is it Signed?

3. Is there a way to give -Offset?

Please check and reply.

Please tell us if you have any further questions.  Thank you.

Comment_SM3320-RF-EV_Schematic.pdf