Part Number: TPS62590
Hi E2E,
I got a strange issue about TPS62590, step down converter. Here below my circuit:
Vin = 5 V and I set feedback network in order to get Vout = 3.3V.
My issue is that the converter shows a 100% duty cycle (does not start to switch), even if the feedback pin is above to 0.6V (0.908V at Vin=5V) and Vout=Vin.
Do you have any suggestions about that.
Thanks in advance.
Antonio Crucito