Other Parts Discussed in Thread: LM73606
A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V , 6A
In the attached circuit diagram, I used 4.7uH of the inductor, and when I contacted E2E, I received a reply saying that there was no problem.
I have already pressed 'Resolved' to the E2E question, so I don't think there will be a reply, so I ask again.
If you calculate with the inductor calculation formula of the Datasheet,
It is about 0.9uH~2.7uH.
(Questions)
1. As mentioned above, please double check that there is no problem even if you apply 4.7uH.
2. If you look at the Datasheet, there is a content related to adding Bulk-Cap to the VIN pin. Is it necessary?
If applied, is there an appropriate capacity value? 100uF or lower capacity possible?