I'm working on a design with a half-bridge consisting of two GaN HEMTs using an LMG1210. As a starting point I took the LMG1210 TINA-TI Reference Design (Rev. C) and let it run. It all worked as expected. However, this design is with a single-ended supply of 50VDC referencing to GND. In my design I need to have a symmetric supply (I chose +/- 25V). Unfortunately, with this in place the design doesn't run anymore, i.e. the gate signals HO and LO remain 0V all the time.
I have tried with a bootstrap circuit and also with a seperate 5V supply for HB, which is referencing to HS. Both didn't work. Is there an issue with the model? Based on the discussion in the E2E forum (LMG1210: Half-Bridge Capability), this mode of operation should be supported if a seperate supply for HB-HS is provided.
Please find attached the modified reference design.LMG1210_ReferenceDesign_modified.TSC