Hello Team,
Good day.
My Customer would like to seek some advice for their application. Using the LM43601PWPR as a positive buck regulator(switcher) to take 13.8 Volts Vin to 3.3V Vout. While testing the design the Bench power supply leads feeding the switcher got shorted together while the switcher was running and providing 3.3 Volts. After the power leads were separated, the switcher failed to regulate and it only outputted 40mV. They do have overvoltage protection on the Voltage input but should they have a reverse biased diode connected across Vin and Vout to prevent back-feeding/reverse discharge of the output voltage into the LM43601 to the Voltage input?
Regards,
Renan