Hi,
the UCD90320 has an embedded sensor which can show the ambient temperature.
1. Looking at the UCD90320 Sequencer and System Health Controller PMBus Command Reference document, there’s a command shown to read an internal temperature sensor. But I can’t find any information in the data sheet on this sensor. Do you know where there might be specifications for it?
2. Can I use this register directly as a logical input of the logical machine which is inside the UCD, so I don't need to read the content from the PMBus?
thanks,
Li