Hi,
I plan to use the TPS61222 in an energy harvesting application that requires a 5V rail with an extremely low power consumption. The 5V rail will be used to drive a CMOS based analog switch whose input will be ~5V. The current used by such a device is not constant and probably hovering close to a few nA.
I selected the TPS61222 because of its very low Iq. My question is whether it will be able to provide a 5V regulated output under almost no load.
Chundra