This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222: Minimum output current for proper voltage regulation

Part Number: TPS61222

Hi,

I plan to use the TPS61222 in an energy harvesting application that requires a 5V rail with an extremely low power consumption.  The 5V rail will be used to drive a CMOS based analog switch whose input will be ~5V.  The current used by such a device is not constant and probably hovering close to a few nA.

I selected the TPS61222 because of its very low Iq.  My question is whether it will be able to provide a 5V regulated output under almost no load.

Chundra

  • Hi Chundra:

    If there is no load, the converter will operate at PFM. The Vout will be a little larger than the target. 

  • Hi Minqui,

    Could you please clarify what PFM stands for?

  • Hi Minqui,

    I would like to use the TPS610997 instead of the TPS61222.  Could you confirm if this is a better device for my application?  Also, I eventually found out that PFM = Pulse Frequency Modulation.

    Section 7.5 of the TPS610997 data sheet mentions that in PFM mode regulation will typically produce 5.15V instead of 5.00V.  However, I could not find any place in the data sheet which explicitly states that the converter is stable with no load.  Could you please confirm if this is indeed the case or if should allow for a bleed current?  If required, what is the minimum bleed current value?

    Chundra

  • Hi Chundra:

    Sorry that I didn't explain it clearly. Yes, the PFM is pulse Frequency Modulation. That's a kind of power save mode to increase the efficiency during the light load. And it can stop the reverse current in most devices.

    The device can be stable both with or without the load. The only difference is it regulate the Vout in PFM is littler higher that normal PWM. 

    I don't have a clear number for when to go into the PFM, as it's related to Vin, Vout, Inductance and other factors. (Generally, <10mA it will operate in PFM, >100mA it will operate in PWM. Just some typical case for your refer.)