This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: ucc2897a clamp mosfet heats and pcb burns

Part Number: UCC2897A
Other Parts Discussed in Thread: PMP22509, CSD19537Q3, TL431

Hello Power Team

we build a board for 5V,5A, using pmp22509 reference design schematic,

i tested this board at 24VDC input voltage and below observation

i) clamp mosfet is heating at 5A load current, upto 3A load current its measured temperature is upto 80°C,

ii) i put this board at 24VDC input voltage and 5V,4A load current in the hot chamber, where temperature is 52°C

after around 2 hours, PCB burnt below and around the clamp mosfet and clamp capacitor burst

 could you help me to resolve this issue

is it any design level issue in the clamp 

the clamp mosfet is FDMC2523P and main swtich mosfet is CSD19537Q3, all other components are also same as reference design PMP22509

we have to run this board atleast at 5V,4A load current in the field at 24VDC input,

may you please guide me on this to help debug the issue

regards

lakh