Hello,
I am trying to understand the behavior of the DRV pin for the UCC28700 flyback controller. The data sheet says the DRV pin is self-limited in both the amount of voltage it can supply and the amount of current it can supply. Does that mean it will attempt to operate at either the maximum voltage (14V), or the maximum current (25mA) at all times, and then self limit accordingly?
Perhaps the following example will help:
When the DRV pin goes high, what is the voltage, and how much current is being supplied?
Best,