Hi Sir,
I can find Over current and Over temperature Protection features in TPS75105 datasheet.
Can you have more detail about these features?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
For the overcurrent protection, the internal current source will sense the output current and when it will trigger OCP protection when the output current is over 35mA;
For over-temperature protection, it will shutdown when it triggered the over-temperature point.
BR
Sean
Hi sea,
Thank you.
I want to know the value of over-temperature point.
BTW, Can we setting the temperature for the over-temperature point?Or it's auto setting from the IC!?
Regards,
Hi Frank.
The over-temperature point is about 165C for the internal junction. It is fixed with some variation as shown on the datasheet on page 5. You can't adjust it by yourself.
BR
Sean
Hi Sean,
Thank you, very helpful.
have a good day!