Hi support team,
After using TPS61161 for half a year, the LED started blinking.
The resistance value between the FB pin and GND is 11.6Ω.
Is TPS61161 damaged and short-circuited?
Please let me know if there is such a precedent.
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support team,
After using TPS61161 for half a year, the LED started blinking.
The resistance value between the FB pin and GND is 11.6Ω.
Is TPS61161 damaged and short-circuited?
Please let me know if there is such a precedent.
Regards,
Dice-K
Hi Dice,
Could you please provide SW, Vout, Iout scope shots for analysis?
In addition, please also make sure that the related capacitors are all OK, especially for Cout.
BR,
Robin
Hi Robin,
Thank you for your reply.
I got the VIN and VOUT waveforms. VIN and VOUT are unstable.
I want to send waveform data as a private message.
The load LCD is a separate board.
The LCD board was inserted and removed many times.
Is it possible that repeated insertion and removal damaged the ESD cell of the FB terminal and caused a short circuit failure?
Best regards,
Dice-K
Hi Dice,
I'll request friendship from you and you can send me these plots.
According to your description--blinking, it seems not a shot circuit issue.
BR,
Robin
Hello Robin,
This is Mochizuki worked together with Dice.
He is going to send you the customers measurement data.
Here is some background information, we have heard from the customer.
They set 4.7mA output current by using Rset 27ohms. Vout was around 8V and initially it works well.
During ES sample evaluation, they plug in-out this LED driver board to LCD backlight module.
After while 2units made strange LED brightness.
They try to measure FB pin resistance as Dice mentioned before. They apply 2.5V high impedance resistance meter.
The result shows some leakage current at FB pin of damaged TPS61161.
Our expectation is that TPS61161 internal ESD cell was damaged by EOS or ESD during hot plug in-out. There is no order GND and Vdd connection at LDC module Flat cable.
And finally ESD cell create large leakage current, then FB circuit function is changed ,LED current is changed from original setting.
The customer agreed if this story is right expectation they will add over voltage protection device to FB pin.
Do you see this story is possible root cause?
Of cause we can go FA to get evidence, apply pin to pin I-V characteristics and if needed apply de-cap package to see ESD cell damage directly.
However it will take time and cost, before fix their mass production product schematics.
Regards,
Mochizuki
Hi Mochi,
Since this issue is a little strange, I will give Dice my email address and you can send me the detailed description. I'll loop in my colleagues to have a further analysis.
Thanks!
BR,
Robin