Other Parts Discussed in Thread: AM5728,
Hi Expert,
custom board AM5728+TPS6590378 can not boot.
I check the signal, pmic will send the reset signal, RESET_OUT(G6) will be low.
What status RESET_OUT will send the reset signal?
Thanks
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
RESET_OUT is released when the power up sequence is complete and one of the following:
• The 16.384-MHz clock is stabilized if the 16.384-MHz crystal is present and the oscillator is enable.
• The external 32-kHz clock is stabilized and the 16.384-MHz oscillator is bypassed.
• The GATE_RESET_OUT_OTP bit is used to allow the TPS659037 device to power up without the
presence of the 16.384-MHz crystal nor the external 32-kHz clock input.
Regards