HI,
I have some questions about tps53681. Can you help me have a look? As follows:
1.What is the default configuration of the chip sent out by the factory? I now have two batches of chips.
One batch has output. The value of the register of 0x02 is 0x17, and the output voltage is 0.8V and 0.9V respectively.
The other batch of chips has no output, and the value of the register of 0x02 is 0x1b
Two batches of chips, register configuration is not the same, so I want to ask the chip factory default configuration is what?
2.What is the PEC of tps53681? Can PEC be closed? If I can shut it down, what should I do?