Hello Team,
I do see some TPS544C25 triggering the over current events.
The current I can measure over PMBus is in the range of 20-24A while over current is set to 40A.
Thus from "steady" current I do not see the over current.
PMBus bandwidth does not allow to measure/detect peak as fast as a comparator would do, so I'm not surprised.
Nevertheless since the steady current is below the OC threshold it meas that is a current peak that trigger the OC event.
The questions:
- Are there ways to measure the current peak that are seen by the OC block?
I do not see anything going out
- What would you recommend to measure the current peak?
- Are there any internal settings/register to enable some delay to allow short peak? Detection window or similar?
only what would last longer would be detected as over current.
Thanks,
SunSet