This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754: Safety certification of CB/IEC 62368-1

Part Number: TPS23754
Other Parts Discussed in Thread: TPS23734

Hi,

May I know whether TPS23754 is certificated with CB/ IEC 62368-1?

Please advise!

Thanks and Best regards,

Tiger

  • Hello Tiger, 

    TPS23754 was released in 2008, and IEC 62368-1 was released in 2014. So it could not have been designed for it. 

    However, TPS23754 does meet IEEE802.3.at, which should comply with IEC 60950, the previous version of that standard. 

    The TPS23734 is the direct replacement for TPS23754, and TPS23734 is 802.3.bt , which i do believe follows IEC62368. Please read the 802.3.at and 802.3.bt standards for further clarification. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments