Other Parts Discussed in Thread: LM5122
Hello
I want use the LM5122EVM-1PH evaluation board to get 15V 10A output from a inpute of 5V (min) to 10V (max), so what components I should change to get thoes specifications ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I want use the LM5122EVM-1PH evaluation board to get 15V 10A output from a inpute of 5V (min) to 10V (max), so what components I should change to get thoes specifications ?
Hi Youcef,
Thank you for your interest in LM5122.
Are you still using the same 250kHz switching frequency?
Thanks,
Yinsong
I might use the same frequency (250 khz) if that possible , but if it better to change it to get my specifications then I will
Hi Youcef,
250kHz should be ok. You will need to change the feedback resistors, UVLO resistors if necessary, and COMP RCs (C25, C26, R25) if necessary.
Please let m know if there is any question.
Thanks,
Yinsong