This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS628502-Q1: FPWM / PFM mode change

Part Number: TPS628502-Q1

Hi,

Can MODE pin controlled after the device is powered up? Back and force between FPWM and PFM dynamically during the device operation. Thank you.

Regards,

Oguri (TIJ automotive FAE)

  • Hi Oguri,

    It is recommended to not leave the Mode pin floating and if you planning to control it with an external signal then I would not expect a critical issue. Could you share how are you planning to control it? 

    However, you can select the mode pin as auto mode so when there is a load device goes into PWM and for the remaining time it will stay in  PWM mode.

     Best rgerds,

    Tanvee

  • Hi Tanvee,

    The customer want the circuit in CCM (FPWM) when the system is active even though the load current is, say 1mA. While, when the system is in sleep, the circuit is in PFM. Thank you.

     

    Regards,

    Oguri (TIJ automotive FAE)

  • Hi Oguri,

    Thanks for the details. I am closing the thread feel free to reach out to us for more details.

    Best regards,

    Tanvee