Other Parts Discussed in Thread: TPS63060
Dear team,
Our TPS63036 has input voltage limit.
Do we have solution, which input range is 2~6V, output 4V/1A and Iq below 25uA?
Many Thanks
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy:
TPS63036 can't handle such load, and can't support Vin>5.5V.
Please check the exactly spec. If customer do need Vin=6V, then you can have a look at TPS63060