This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3895: CS pin reaction

Part Number: UCC3895

Dear Team,

When the CS pin larger than 2.5V trigger the protection, the circuit will latch, cycle by cycle limit, or soft start?

Besides, can I give the CS pin a DC value?

BR

Kevin

  • Hi, Kevin

    When the CS pin larger than 2.5V trigger the protection, the controller will restart with soft start.

    It is not recommended to give CS pin a DC value. Since it peak current mode, the signal on CS pin affect effective duty. 

    BR,

    Yunsheng