Dear all, good morning.
I am trying to simulate a resonant converter using Test_LMG3410_BUCK design example as starting point, just replacing LMG3410R150 with the LMG3410R050. Apart from that, the switching frequency was changed to 500kHz and the power-side voltage to 50V, but the rest of the circuit remains unaltered.
When I test the half-bridge with no load or resistive one, I obtain the desired square waveform. However, when I connect the resonant circuit, the output waveform just do not make sense.
Doing some desperate trials, I realize that including an isolated voltage source (as shown in the following picture) makes the system work as desired. Nevertheless, it seems that including this component is not right as I cannot analyze the effects produced by the resonant circuit in the switches.
It is important to say that the resonant circuit was also tested with sinusoidal and square-wave voltage source, and it is working as expected.
Any suggestion regarding this issue will be highly appreciated! Thank you all in advance.