Other Parts Discussed in Thread: LM34936, LM5170
Hi,
i need information for the below queries
1.we need buck boost controller for high power rating , please find the below voltage and current rating .
VIn=6 to 36V
Vout=12V to 25V
Iout=24V@45A (continuous)
Efficiency : more than 95%
if you have any part support more than 30A also please suggest.
2.And one more query is ,LM34936 can design up to 40A to 50A @24V? if it support please suggest the design consideration.
Regards,
Rudraprasad.V