This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61310: LED2 output current issue

Part Number: TPS61310

Hi Sirs,

My customer tries to set the LED2 current to 700mA, but they only measure the 340mA current on LED2. How to fix this issue?

schematic:

F/W setting value:

static void StartTPS6105XFlash(U8 byIntensity)

{

          XBYTE[PG_GPIO_AL_CTRL0]  &= ~GPIO_AL2_DRIVING_HIGH;

 

          WriteTPS6105XReg(0x03, 0x73);

          WriteTPS6105XReg(0x05, 0x6F);

          XBYTE[PG_GPIO_AL_CTRL0] |= GPIO_AL0_DRIVING_HIGH;

         

          WriteTPS6105XReg(0x01, 0x1C); // LED 2 = 700mA

          WriteTPS6105XReg(0x02, 0x9F); // LED1/3 = 400mA

         

}


LED1 current waveform:

LED2 current waveform:


LED3 current waveform: