Hi team,
We would like to recommend this solution to customer but there is one question from customer.
Need team's explanation and clarification.
Output spec:
1. Vo= 0.9V/3.904A
2. Vo= 0.8V/ 3.3A
Input voltage:
Customer will use 1.1V as input voltage but they should consider the1.1V has 3% tolerance (1.067V~1.133V), so is there any concern?
The Vbias they could use either 3.3V or 5V.
their Vo ripple voltage demand: <=2mV.
Or do you have another suitable solution for suggestion?
Thanks