This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2113A: Recommendation to connect two TPS2113A switches in parallel ideally or does exist alternative switch with higher current?

Part Number: TPS2113A
Other Parts Discussed in Thread: TPS2121

Dear Sir or Madam,

my question regards to set two TPS2113A in parallel to get a higher current delivery. Unfortunately I cannot find an alternative switch with the same conditions but with a higher current of approx. ~3.5A.

I want to use the VSNS comparator to decide the switching process through different input voltage levels. But if two switches are working parallel there are two comparators which has to be feed with one resistor divider. I guess through the tolerances the switching process will not work synchron. Correct?

Do you have some experiences to interconnect parallel two TPS2113A with a optimal synchronisation? Can you give some advices/recommendations?

Of course I am open for an alternative switch but I cannot find an identical one with a higher current delivery.

Thank you very much beforehand.

Best regards

Wolfgang Walter