Other Parts Discussed in Thread: BQ78350
Hello;
I note that there are numerous gaps between parameter offsets in the Flash. Are there hidden variables which if clobbered, may/will result in unpredictable or faulty behavior? I found this to be true in the bq78350's DF, and so I'm assuming its also true with the 34z100 (?).
For example, the parameters "Ra Filter" sits at offset 17 in sub-class 80, and the next parameter "Min PassedChg NiMH-LA 1st Qmax" sits at offset 47
When reading sub-class 80, are the hidden bytes of significance? For ex., note the 8 bytes loaded into fill1 below...do they mean anything? or are they simply random ?