This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116FEVM-571: Control with LabView

Part Number: TLC59116FEVM-571
Other Parts Discussed in Thread: TLC59116F, TLC59116

Hi,

For my current project I am using the TLC59116F EVM-571. Instead of using LED's I connected small Peltier Elements and control them with the supplied Software.The Peltier Elements are connected only to the Pins which belong to the Blue Part of LED's (Peltiers are soldered to jumper wires and then connected to the board). The temperature of the peltier elements is controlled by setting the blue value between 0 and 255 in the supplied software. This software does not fit the requirements and make some problems. Hence, the idea is to use LabView. All I need to know is if there is the possibility to control and access this device with LabView, are the proper LabView Drivers, what do I need etc.

Best regards,

Johannes

  • Hi Johannes,

    We do not have existing LabView driver for this device. But TLC59116 support standard I2C protocol, which is very common protocol in low speed device. I think LabView should have public resource for it.