Is there p2p compatible with TPS76150 since customer is looking for higher voltage up to 20Vin?
Condition:
Input Voltage: +15V, 5% accuracy
Output Voltage: 5V
Output Current: <20mA
Application: Current Module
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there p2p compatible with TPS76150 since customer is looking for higher voltage up to 20Vin?
Condition:
Input Voltage: +15V, 5% accuracy
Output Voltage: 5V
Output Current: <20mA
Application: Current Module
Hey Brian,
Thankfully TPS761 uses a pretty standard pinout for the SOT-23 package so we have a few options. My first suggestion would be TPS709 since it has a max Vin of 30V and has reverse current protection. If they don't need the reverse current protection then TPS7A24 would also be an option with the Recommended Max Vin is 18V with an Abs Max of 20V.
Below is a quick comparison between the three parts.