Hi
after reviewing the schematic I ASSUME I change R1 for higher current. However it is a single diode VF = 1.8V @ 1.5A. Most of your applications are or boost configuration for more than 1 LED. The evm datasheet does not address the buck portion of the schematic. Is this part appropriate for my application: single diode, VF =1.8V @ 1.5A for 3msec 30Hz dc or 1.5A for 1msec 3Hz? Can you help me modify the evm for this application. This is a application for testing in a laboratory so I would prefer to modify an evm rather than design a board around it which can be done but in the interest of time...
Thanks