Hi,
If a fet is NOT used to disconnect Bat from Pack+ ,
- Can LD or PACK pin be used to detect a charger and wake the chip from shutdown mode when its connected by looking at the rising edge ?
- Can LD pin left floating if its not used? Any issues with leaving it floating ?
- Should PACK pin left floating ? Any issues with leaving it floating ?
- Section 13.3 of datasheet, says. "If the PACK pin voltage is higher than the top-of-stack voltage by more than a programmable delta and the top-of-stack voltage is less than a programmed threshold, the device will exit SLEEP mode." . What is the intention of the second condition, when its less than a programmed threshold ?