Hello, 2> Could you confirm this calculation is also usable for the TLC5943 , as this calculation is not Included in the doc ?
My customer wouldlike cascading up to 160 Chips ,60Hz refresh .
Datasheet of TLC5945 (SLVS755) , page18 , give F(SCLK) mini = 193 x 160 x 60 = 18 852 800 hz
That is far under the Max clock of 30Mhz of TLC5945 .
1> How to explain the sentense page18 : ?
<The maximum number of cascading TLC5945 devices depends on the application system and is in the range of 40 devices>
(this is to have possibility to use the 16Bits PWM)
Thanks for Help,
Michel VINEZ DFAE