Hi,
Based on 8.3.6 of LMR14030, I can calculate RENT and RENB for desired UVLO hysteresis voltage. My questions are:
1. Is the VSTART the same as UVLO_H, and VSTOP is the same as UVLO_L?
2. Can I use RENT and RENB to set VSTART to be 8V and VSTOP to be 7V? Since based on the datasheet, the max value of UVLO is 3.9V.
Best regards,
Tianze