Other Parts Discussed in Thread: BQ24075
Hi,
I am using BQ227441 in addition with BQ24075.i am using Bq27441 for the past 2 days and it worked fine for 2 days but suddenly BQ27441 stopped communicating with my controller which is connected externally through I2C, So i started debugging and noticed that i was not getting 1.8V at VDD pin and getting something else like in attached picture and waveform at GPOUT is also attached.
First Attachment : VDD,
Second Attachment : GPOUT.
Battery Voltage is 3.96V connected to BQ27441.
Thanks & Regards,
P.Akhil.