Hi,
LM43603-Q1 is designed with input voltage range is from 9V to 36V and output is 5V in my customer's board.
RT pin of LM43603-Q1 is connected with a resistor to make 990KHz switching frequency.
The resistor value is 40.2Kohm and it has 1% tolerance.
But, measured switching frequency is 870KMHz.
This has an 12% error.
In the datasheet, Frequency adjust accuracy is 10% and I know that it is typical value.
What is the max tolerance switching frequency of LM43063-Q1?
Is 12% error normal?